One family houses

  • Record savings on central heating consumption

     'When we bought the new living solution, we were told it could save us 23% on energy consumption. After one year with living we can see that we have actually saved almost 38% - and we expect our heating bills to remain at this low level from now on, year after year.'

    Birgit,
    Export Engineer,  Køge

  • No need to turn the heat up and down

    It is a relief for the family to not have to turn the heat up and down in each individual room: this happens completely automatically. All rooms can be set to a basic temperature, reduced nighttime temperature, etc. from the central Link panel. Should something need hanging, this can be done with a simple press of the button for the room currently listed on the panel, after which the temperature is reset at the new level.

    “The automatic control means that we always have the right temperature in each individual room. We are pleasantly surprised by how precise Danfoss living connect® thermostats are, and how quickly they react to changes in room temperature,” explained Birgit.

    When the family goes on holiday, they simply give the Link panel a message that they are away, and the temperature is then reduced in all the rooms, and raised again so that it is nice and warm when the family return home.

     

  • Quick and easy installation

    It took just one morning to get the Køge family’s new living solution up and running. The qualified installer arrived in the morning and replaced all the radiator thermostats with the new living connect® thermostats in a smart, simple and easy-to-clean design, after which all the thermostats were connected to the central Link control and set to the desired temperatures.

    Three hours later, it was all working perfectly.

     

     

Be social Take part

Want to socialize with us?

Get to know us and take part in the conversation